我下载的是ti-processor-sdk-rtos-k2hk-evm-04.03.00.05-Windows-x86-Install.exe,
在我运行BenchmarkProjectCreate.bat时,
报错:SDK build environment not setup.run setup script in root Processor SDK RTOS directory.
请问我应该怎么解决呢?谢谢。怎么设置该SDK环境呢?
66AK2H,根据指示software-dl.ti.com/.../Overview.html
在Windows下
From the RTOS SDK directory, enter
C:\ti\processor_sdk_rtos_[soc]_[version]> setupenv.bat
之后显示PROCESSOR SDK BUILD ENVIRONMENT CONFIGURED
随即运行gmake,显示createprocess failed。
然后我再到demos中任意一个demo运行projectcreate.bat,说我SDK build environment not setup.run setup script in root Processor SDK RTOS directory.