AWR1443BOOST:Vital Signs Data phase unwrap



您好:

根据Matalb GUI代码,从Vital Signs Lab记录的bin文件中取出了Range Profile以及Phase,后面需要进行unwrap。我对这一过程有一些疑问:

1、代码中unwrap过程为 ant1_Ph = angle(rangeProfile_cplx(row_index,:));         ant1_UnWrapPh = unwrap(ant1_Ph);

每一帧时间为10个chirp的时间,但是只配置了两个chirp,文件记录下了这两个chirp的数据,其他数据为0,unwrap是否应该去除这些为0的数据?

2、在DevelopmentGuide中说明,Each chirp is configured to have 2 chirps. However only the 1st Chirp in the frame is used for processing。和上个问题一样,这是否说明只对每一帧的第一个Chrip数据进行unwrap,去除第二个chirp以及其他为0的数据?

3、实际实验中,理论的数据时间与我实验时间对不上。我连续采集了大概有150s左右的数据,但是最后只包含5000组数据(包括为0的),对应500个frame,则理论时间为500×0.05s=25s,请问是什么原因?