DRV8702-Q1在SLEEP模式下SH-x不是Hi-Z高阻态问题咨询

Other Parts Discussed in Thread: DRV8702-Q1

我最近在测试PLG项目中使用的DRV8702-Q1时发现SH-x管脚并不是Hi-Z模式,请问这个是为什么?SH-x管脚的内部阻抗(或者灌电流)的范围是多少?
    我测试时将DRV8702-Q1设定在下图的模式下:
    测试的原理图如下:
    我测试了在DRV8702在Sleep模式下,将S_HS2的高驱输出情况下,测试 原理图中A/B/C/D四点在输出线带电机,不带电机,带电机后输出线对电源短路,带电机后输出线对地短路四种情况下的电压,测试了两块板子(每块3个DRV8702)的数据如下:
Board Number-Motor type VB power supply Motor Status TP516 X2-1 X2-2 V_motor1_status_AD_P96(TP548) Board Number-Motor type VB power supply Motor Status TP516 X2-1 X2-2 V_motor1_status_AD_P96(TP548)
#1-Motor1 DRV8702
MOD=Hi-z SLEEP status 
8.5 Connect Nomal 7.09 1.398 1.398 0.355 #2-Motor1 DRV8702
MOD=Hi-z SLEEP status 
8.5 Connect Nomal 7.14 1.403 1.403 0.356
OPEN 7.09 2.081 0 0 OPEN 7.15 2.093 0 0
Short to Power 8.42 8.43 8.43 2.12 Short to Power 8.46 8.47 8.47 2.133
short to Ground 7.08 0 0 0 short to Ground 7.13 0 0 0
14.5 Connect Nomal 13.08 2.19 2.19 0.554 14.5 Connect Nomal 13.05 2.187 2.186 0.555
OPEN 13.09 3.494 0 0 OPEN 13.06 3.488 0 0
Short to Power 14.45 14.46 14.46 3.631 Short to Power 14.42 14.43 14.42 3.637
short to Ground 13.06 0 0 0 short to Ground 13.04 0 0 0
16.5 Connect Nomal 15.02 2.446 2.445 0.619 16.5 Connect Nomal 15.03 2.451 2.45 0.621
OPEN 15.02 3.945 0 0 OPEN 15.04 3.96 0 0
Short to Power 16.41 16.42 16.42 4.12 Short to Power 16.41 16.42 16.43 4.13
short to Ground 15.01 0 0 0 short to Ground 15.02 0 0 0
Board Number-Motor type VB power supply Motor Status TP604 X2-3 X2-6 V_motor1_status_AD_P93(TP633) Board Number-Motor type VB power supply Motor Status TP604 X2-3 X2-6 V_motor1_status_AD_P93(TP633)
#1-Motor2 DRV8702
MOD=Hi-z SLEEP status 
8.5 Connect Nomal 7.09 1.403 1.402 0.35 #2-Motor2 DRV8702
MOD=Hi-z SLEEP status 
8.5 Connect Nomal 7.15 1.415 1.415 0.356
OPEN 7.1 2.101 0 0 OPEN 7.16 2.124 0 0
Short to Power 8.45 8.45 8.45 2.122 Short to Power 8.46 8.47 8.47 2.126
short to Ground 7.07 0 0 0 short to Ground 7.13 0 0 0
14.5 Connect Nomal 13.07 2.2 2.2 0.549 14.5 Connect Nomal 13.05 2.204 2.203 0.554
OPEN 13.08 3.53 0 0 OPEN 13.06 3.54 0 0
Short to Power 14.45 14.46 14.46 3.603 Short to Power 14.42 14.43 14.43 3.619
short to Ground 13.06 0 0 0 short to Ground 13.04 0 0 0
16.5 Connect Nomal 15.02 2.459 2.458 0.614 16.5 Connect Nomal 15.02 2.468 2.467 0.62
OPEN 15.03 3.999 0 0 OPEN 15.04 4.02 0 0
Short to Power 16.41 16.42 16.42 4.09 Short to Power 16.41 16.42 16.42 4.12
short to Ground 15.01 0 0 0 short to Ground 15.01 0 0 0
Board Number-Motor type VB power supply Motor Status TP637 X2-4 X2-10 V_motor1_status_AD_P92(TP667) Board Number-Motor type VB power supply Motor Status TP637 X2-4 X2-10 V_motor1_status_AD_P92(TP667)
#1-LOCK DRV8702
MOD=Hi-z SLEEP status 
8.5 Connect Nomal 7.09 1.414 1.414 0.356 #2-LOCK DRV8702
MOD=Hi-z SLEEP status 
8.5 Connect Nomal 7.15 1.411 1.41 0.355
OPEN 7.1 2.113 0 0 OPEN 7.16 2.116 0 0
Short to Power 8.45 8.45 8.45 2.12 Short to Power 8.47 8.47 8.47 2.13
short to Ground 7.14 0 0 0 short to Ground 7.14 0 0 0
14.5 Connect Nomal 13.08 2.209 2.209 0.555 14.5 Connect Nomal 13.06 2.197 2.196 0.553
OPEN 13.09 3.551 0 0 OPEN 13.07 3.526 0 0
Short to Power 14.45 14.45 14.45 3.627 Short to Power 14.42 14.43 14.43 3.626
short to Ground 13.07 0 0 0 short to Ground 13.05 0 0 0
16.5 Connect Nomal 15.04 2.472 2.471 0.621 16.5 Connect Nomal 15.04 2.459 2.458 0.619
OPEN 15.05 4.02 0 0 OPEN 15.05 4 0 0
Short to Power 16.41 16.42 16.42 4.12 Short to Power 16.4 16.41 16.42 4.13
short to Ground 15.03 0 0 0 short to Ground 15.02 0 0 0


    通过观察上述数据可以发现在OPEN下A点与B点有很大的压差,则说明DRV8702的SH-x管脚并不是Hi-Z的高阻态。

    综上所述:
    我想知道SH-x管脚的内部阻抗(或者灌电流)的范围是多少?因为这个会影响我的电机诊断的阈值,