可以的, PGAxxxEVM-034 板适用于PGA900, PGA300, PGA305. 在PGAxx EVM user's guide 上也有相应描述:
The PGAxxxEVM-034 supplies a platform to test the PGA900, PGA300, and PGA305 in the QFN package. The EVM is shipped as either the PGA900EVM-034, the PGA300EVM-034, or the PGA305EVM-034, with the name identifying the signal conditioner included in the EVM package. The PGAxxxEVM-034 supplies an interchangeable platform all of these devices can use.