IWR1642 DEMO问题



我使用toolbox里面自带的.bin文件,雷达可以正常运行,但是当我使用开发者模式,编译DEMO提供的代买之后,使用编译生成的.bin文件,雷达却无法正常运行,没有图像,这是为什么?

  • 你好,

    请问你编译的是哪个demo,哪个版本?

    需要看一下user guide是否有软件版本的要求。比如people counting的下列库。

    ToolVersionRequired ForDetails
    mmWave Industrial Toolbox 2.2.0+ - Contains all files (quickstart, visualizer and firmware source files) related to mmWave People Counting Lab
    TI mmWave SDK 1.02.00.05+ Firmware Source Code The latest TI mmWave SDK and all the related tools are required to be installed as specified in the mmWave SDK release notes
    Code Composer Studio 7.4+ Firmware Source Code Download link Note: CCSv6.x cannot be used
    C6000 Code Generation Tool 7.4.16 Firmware Source Code To compile code for the DSP core(C674x), the version 7.4.16 compiler must be installed under C:\ti. Download link
  • 我使用的是ppcount demo,toolbox版本是2.3,SDK是1.25,
    我用的是CCS8.0 ,不过我CGT选择7.4.16的话,编译会失败,我选择的CGT是8.1.3,虽然编译成功了,但是烧.bin文件进板子之后,依然无法正常运行,没有图像
  • 你好,
    必须选用7.4.16,8.1.3编译成功后,现象的确是没有点输出。仅支持7.4.16
    建议重新导入工程进行尝试,另外,请检查其他的几个编译组件,是否都满足user guide中的描述?
    谢谢。
  • 您好,如果我选择CCS7,并用CGT7.4.16的话,编译器会报错 报错如下:
    **** Clean-only build of configuration Debug for project pplcount_16xx_dss ****

    "E:\\Program Files\\CCS7.4\\ccsv7\\utils\\bin\\gmake" -k -j 8 clean -O

    DEL /F "xwr16xx_pplcount_dss.hex" "configPkg\linker.cmd" "configPkg\compiler.opt" "xwr16xx_pplcount_dss.xe674"
    RMDIR /S/Q "configPkg\"
    DEL /F "RADARDEMO_aoaEstCaponBF.oe674" "RADARDEMO_aoaEstCaponBF_DopplerEst.oe674" "RADARDEMO_aoaEstCaponBF_heatmapEst.oe674" "RADARDEMO_aoaEstCaponBF_matrixInv.oe674" "RADARDEMO_detectionCFAR.oe674" "RADARDEMO_detectionCFAR_priv.oe674" "RADARDEMO_rangeProc.oe674" "RADARDEMO_rangeProc_priv.oe674" "RADARDEMO_rangeProc_utils.oe674" "cycle_measure.oe674" "dss_config_edma_util.oe674" "dss_data_path.oe674" "dss_main.oe674" "radarOsal_malloc.oe674" "radarProcess.oe674"
    DEL /F "RADARDEMO_aoaEstCaponBF.d" "RADARDEMO_aoaEstCaponBF_DopplerEst.d" "RADARDEMO_aoaEstCaponBF_heatmapEst.d" "RADARDEMO_aoaEstCaponBF_matrixInv.d" "RADARDEMO_detectionCFAR.d" "RADARDEMO_detectionCFAR_priv.d" "RADARDEMO_rangeProc.d" "RADARDEMO_rangeProc_priv.d" "RADARDEMO_rangeProc_utils.d" "cycle_measure.d" "dss_config_edma_util.d" "dss_data_path.d" "dss_main.d" "radarOsal_malloc.d" "radarProcess.d"
    找不到 C:\Users\DeapOcean\workspace_v7\pplcount_16xx_dss\Debug\xwr16xx_pplcount_dss.hex
    'Finished clean'


    **** Build Finished ****

    **** Build of configuration Debug for project pplcount_16xx_dss ****

    "E:\\Program Files\\CCS7.4\\ccsv7\\utils\\bin\\gmake" -k -j 8 all -O

    rm -f C:/Users/DeapOcean/workspace_v7/pplcount_16xx_dss/xwr16xx_pplcount_dss.bin
    makefile:199: recipe for target 'pre-build' failed
    process_begin: CreateProcess(NULL, rm -f C:/Users/DeapOcean/workspace_v7/pplcount_16xx_dss/xwr16xx_pplcount_dss.bin, ...) failed.
    make (e=2): 系统找不到指定的文件。

    gmake[1]: [pre-build] Error 2 (ignored)

    'Building file: "../dss_mmw.cfg"'
    'Invoking: XDCtools'
    "E:/Program Files/CCS7.4/xdctools_3_50_04_43_core/xs" --xdcpath="C:/ti/bios_6_53_02_00/packages;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C674 -p ti.platforms.c6x:IWR16XX:false:600 -r release -c "C:/ti/ti-cgt-c6000_8.1.3" "../dss_mmw.cfg"
    subdir_rules.mk:103: recipe for target 'build-1994956399-inproc' failed
    E:/Program Files/CCS7.4/xdctools_3_50_04_43_core\packages\xdc\bld\xdc.mak:238: *** can't find specified XDCROOT: E:/Program Files/CCS7.4/xdctools_3_50_04_43_core. Stop.
    js: "E:/Program Files/CCS7.4/xdctools_3_50_04_43_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
    gmake[2]: *** [build-1994956399-inproc] Error 1
    gmake[1]: *** [build-1994956399] Error 2
    gmake[1]: Target 'main-build' not remade because of errors.
    subdir_rules.mk:100: recipe for target 'build-1994956399' failed
    makefile:165: recipe for target 'all' failed
    gmake: *** [all] Error 2

    **** Build Finished ****
  • 你好,

    能否尝试将CCS及demo都放置与默认路径?再进行编译?

    谢谢。

  • 您好,你的CGT7.4.16是自带的吗,我使用sdk安装完之后是8.1.3

  • 你好,
    7.4.16需要独立安装。链接如下:
    software-dl.ti.com/.../download.htm