OPT8320的设计参考及其建议

Other Parts Discussed in Thread: OPT8320, TPS2559

各位大佬,

本人拟采用OPT8320进行相应系统设计,由于没有看到OPT8320的参考设计,只有查阅OPT8241的EVM板资料进行相应系统设计。目前存在如下几个疑问,希望能够有人提供解惑和建议:

1、在OPT8241 EVM上采用的TPS2559恒流源的电流控制是由外部I2C(即FX2上的I2C)控制的(控制反馈电阻阻值得以实现),那么这一块的电流控制原理及程序,有什么建议?在OPT8320上是否也是参照这个方法设计?

2、在OPT8241 EVM板上的光学调制信号,其中激光管电流由ILLUM_P控制,而六颗LED管的电流调制由ILLUM_N控制,这里有什么讲究和建议?

3、在OPT8241 EVM板上的SUB_BIAS由两颗MOS管组成的反馈电路输入,而OPT8320的Datasheet上的各种数据表格中都是指定为0V,在实际系统中,MOS管反馈电路有什么好处?是否直接接地或者通过磁珠接地是否可以?有什么风险?

4、在OPT8320上增加了ILLUM_PWM_CTRL/ILLUM_PWM_SYNC管脚,这两个管脚什么作用?是否也是起到恒流源的功率控制作用?如果是,有没有建议的参考电路?

5、OPT8320上MOD_CDRIV/VSS_CDRIV管脚可以提供150mA的调制电流,如果直接采用该管脚控制LED/激光管,大概能达到的测量距离是多少?如果采用建议的SFH4715S/SFH4232等电流较大的LED,这个调制电流源是否就不能用了?如果不用该管脚,是否悬空即可?还是有什么建议?

6、OPT8320数据手册中,参数表中MIXH都是建议典型值为1.5V,而其他参数表的测试条件大多数在1.8V,从设计简化角度,我将使用1.8V,想了解这个1.8V的纹波有多大,即是否要彻底与其他1.8V分开,还是能够采用一个磁珠隔离即可?

7、外部温度传感器是要要靠近恒流源芯片,还是LED/激光管器件?布局有什么建议?

8、(可能是原理性问题,或者我没有理解)在ToF系统设计文档中,抽象了恒流源输出调制电路原型,在ILLUM_P控制下切断电流是,MOS管是直接连接到旁路电路,在这个旁路上只有电感,没有其他更多吸能的电阻或者器件,是否会有电路工作风险?(短路或者其他)

应骏