1642 ES2.0支持的flash有9种,最初使用的是MX25V1635FZNQ,如果更换成W25Q16DVZPIG或者S25FL132K0XNFB01的话,需要做些什么工作呢?
1642 ES2.0支持的flash有9种,最初使用的是MX25V1635FZNQ,如果更换成W25Q16DVZPIG或者S25FL132K0XNFB01的话,需要做些什么工作呢?
你好,
器件支持并测试过以下型号flash。如果想换为其他型号flash,建议使用QE位(四线模式)出厂即enable的型号,
同时如果是来自其他供应商的flash型号,有两点要求:
本地团队测试过W25Q032FVSIG在手动把QE设置为1后,即可被1642支持。GigaDevice GD25B64C可直接使用。
The AWR1243/XWR1443 devices have only been tested with Spansion and Macronix devices. The flash variants that have been tested are as follows:
Flash Vendor Variant Remarks
CYPRESS (SPANSION) S25FL132K0XNFB01 QE bit set by ROM bootloader in SOP5 while flash programming
CYPRESS (SPANSION) S25FL256S QE bit set by ROM bootloader in SOP5 while flash programming
CYPRESS (SPANSION) S25FL064LVF01 QE bit set by ROM bootloader in SOP5 while flash programming
MACRONIX MX25L3233F QE bit set by ROM bootloader in SOP5 while flash programming
MACRONIX MX25R1635FZNIH0 QE bit set by ROM bootloader in SOP5 while flash programming
MACRONIX MX25V1635FZNQ QE bit set by ROM bootloader in SOP5 while flash programming
MACRONIX MX25U1633FZNQ QE bit set by ROM bootloader in SOP5 while flash programming
MACRONIX MX25V8035FM1Q QE bit set by ROM bootloader in SOP5 while flash programming
ISSI IS25LQ016B-JBLE By setting QE bit externally once
ISSI IS25LP080D QE bit set
WINBOND W25Q16DVZPIG By setting QE bit externally once