IWR1642 BOOST 天线角度问题

Other Parts Discussed in Thread: TIDEP-0090, IWR1642BOOST

你好,在TI Resource explorer 中的Antenna Database中显示视场是120和30度,在TIDEP-0090中说的是100和22,请问后面的角度仿真是基于76.5GHZ的吗?

如果使用76GHZ-77GHZ频段,是以100和22为准吧,怎么理解

谢谢

  • 你好,
    请参考:
    e2e.ti.com/.../658632

    The IWR1642BOOST EVM has an elevation FOV of about +/- 15 degrees so a total of about 30 degrees (based on 6 dB drop in the gain as compared to bore sight). You can refer to the antenna pattern plot in section 2.6 of the IWR1642BOOST user guide.
x 出现错误。请重试或与管理员联系。