TDC7201 trigger信号问题

Other Parts Discussed in Thread: TDC7201

我在使用贵司的TDC7201芯片用于激光测距,目前,我采用的是测量模式1(measurement mode 1),使用单次测量时,芯片能够正常工作,clock_count寄存器、校准寄存器1、2都能读取到数据,完成中断信号也是正常的。但在尝试多测平均测量的方式(multi-cycle averaging)时遇到了一些问题:我配置了TDCx_CONFIG1的TRIGG_EDGE,TDCx_CONFIG2的AVG_CYCLES,之后置位了TDCx_CONFIG1的START_MEAS位进行测量,发现多次测量的方式并没有正常工作,单片机引脚没有捕获到trigger信号。我的寄存器配置是:TDCx_CONFIG1 = {0x01},TDCx_CONFIG22 = {0x50}。请问,这个模式使用是否有什么需要注意的,以及在模式1下能否使用该模式?