Customer use this PN, found that ADC temperature is more higher than room temperature, and customer test static power is more higher than datasheet, is about 250mW, so is there any advise for this design, Thank you.
您好, ADS804E芯片温度大概多少呢,功耗您是怎么测得呢,采样率多少呢,我看图中使用的是外部参考电压2.5V,VREF也是2.5V,输入范围是0~5V,而数据手册给出的功耗200mW(max)是在输入范围1.5V~3.5V情况下测的,测试条件不同,功耗有少许不同应该也正常。
您好,客户是在空载状态下测试出来的,温度超出室温,发热就比较严重。
您好,这边测试的是未加任何输入(包括CLK)测得功耗是300多将近400毫瓦的功耗,测试方法是在一块裸板上只焊一片ADS804E,供电5V,这样测出来的跟在装置上测得静态的时候的功耗是基本差不多的,因此我认为这应该不是输入信号的范围的问题。