DRV8837DSGR低温下无输出,是哪里的原因,不是物料有问题?

Other Parts Discussed in Thread: DRV8837

1.测试过程中发现有2个ID出现卡堵,工程师试着将驱动器拆开,将驱动芯片(DRV8837DSGR)的输入信号及输出信号引线出来,用示波器测试运行的波形,发现在-40℃时驱动芯片的输入信号是有的,但是没有输出信号。

2.将此样品寄回本量后,低温不转的现象是可以复现的,常温降温至-40℃时还能正常工作,在-40℃保持20分钟左右再设角就电机不转,从-40℃升温过程中,升至大概在-20℃又能工作

3..将不良DRV8837DSGR取下,焊至另外一台正常样机上,在低温-40℃仍然不良,而更换另一个批号到原不良的位置,-40℃工作正常