请问关于DRV8886步进电机驱动芯片问题



外设与规格书一致,decay除外,decay我直接用10k电阻下拉,rref电阻用30k电阻下拉接地,从理论上计算IFS应该是1A,但我实际电流才40mA,发现VCP有波动,并且与fault低电平变化位置一致,改变VCP与VM连接电容后,VCP电压变平缓,但fault低电平占空比更大,电容改为0.1UF时,电流为80mA,但无论怎么改变电容也不能再进一步增大电流,在AOUT1和BOUT1上串联10-100欧姆电阻,电流会在80到500mA变化。