求助:PGA970和XDS200连接不上

Other Parts Discussed in Thread: PGA970

各位:

我用了自己设计的PGA970板,XDS200仿真器 CCS7.0。连接的时候总是报错  后来在自己的电脑上不知道怎么折腾好了  可以连接  就是成功率比较低 总是报错 让我降低通讯速率。

换任何一台其他电脑都无法连接成功

一直在报错‘-183’

请问有人遇到过类似问题吗??

-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Feb 13 2017'.
The library build time was '15:28:48'.
The library package version is '6.0.576.0'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-183' (0xffffff49).
The title is 'SC_ERR_CTL_CBL_BREAK_FAR'.
The explanation is:
The controller has detected a cable break far-from itself.
The user must connect the cable/pod to the target.
[End: Texas Instruments XDS2xx USB Debug Probe]