Other Parts Discussed in Thread: PGA460
PGA460的开发板,GUI界面按照数据手册配置不好,数据手册只是例子么,为何按照数据手册上的图片内容配置,仍然不能测出距离,望解答,麻烦了谢谢。
你好,这边可以通过GUI配置好测量出距离了,但是还有些问题,我如果只用上半部分的PGA460板子和stm32通过串口连接驱动,而不用下面的MSP430,那么需要PGA460的哪些引脚呢,需要如何配置呢,数据手册里面应该有,但是太多了没有找到。。。谢谢麻烦解答了
很简单的,PGA460的第10脚和第11脚连接mcu的uart接口就好了。或者找到你PGA460板子的原理图,把和msp430连接的引脚替换到stm32上就好了。
这边已经测试过了,我先使用msp430+PGA460这一套开发板然后配合着stm32发送指令可以接收到芯片返回的数据,但是去掉msp430单独使用PGA460再用stm32就接收不到数据了,请问是什么问题呢?麻烦了谢谢,可以加一下您的qq联系方式么?
这边可以接收到了不是程序的问题,得把3.3V和5V都接上才可以工作啊,已经可以返回数据了,麻烦了哈哈
GUI能直接和PGA460板子通讯吗在不使用msp430这块板子的前提下