DRV8432芯片的VDD和GVDD使用的12V电压需要多大的功率?



DRV8432芯片的VDD和GVDD使用的12V电压需要多大的功率?

  • 感谢您对TI雷达波产品的关注!我们正在跟进您遇到的问题。由于国庆长假期间,中文论坛支持将会有所延迟。您也可以关注下帖,我们E2E英文社区的TI专家会进行回复。

    https://e2e.ti.com/support/motor-drivers/f/38/t/843560

  • 请参考数据表的8.2.1.2.2:
    "The DRV83x2 requires a 12-V power supply for GVDD and VDD pins. The total supply current is relatively low at room temperature (less than 50 mA), but the current could increase significantly when the device temperature goes too high (for example, above 125°C), especially at heavy load conditions due to substrate current collection by 12-V guard rings. TI recommends designing the 12-V power supply with a current capability at least 5-10% of the load current, and no less than 100 mA to assure the device performance across all temperature ranges."

    示例:如果DRV8432设计为在14A条件下连续工作,则GVDD / VDD电源的额定电流应为1.4A。