Other Parts Discussed in Thread: LMP91000
各位前辈大家好,小弟正在做一个测气体浓度的项目,要用到LMP91000这款芯片,我在网上下载到了其基于MSP430单片机的code,程序一开始就对LMP91000进行设置,命令是0X48,我知道0X48是91000的地址,我的问题是难道直接写入地址,不用写入任何命令就可以从01--12中读取数据吗?然后后面又是写入0X00,写入0X18,让我不太理解,请用过的前辈为我解答一下,谢谢。
I2CSetup(LMP91000_I2C_Address); (0X48) // Initialize I2C modul
TI_LMP91000_MENB_PxOUT &= ~TI_LMP91000_MENB_PIN; // Enable \MENB Pin
TI_LMP91000_MENB_PxDIR |= TI_LMP91000_MENB_PIN; // Set pin direction is outpu
while (status == TI_LMP91000_NOT_READY) (0X00) // wait while device is not ready
status = LMP91000_I2CReadReg(TI_LMP91000_STATUS_REG); (0X00) // Read device ready status
read_val[0] = LMP91000_I2CReadReg(TI_LMP91000_LOCK_REG); (0X01) // Read from lock register default value
read_val[1] = LMP91000_I2CReadReg(TI_LMP91000_TIACN_REG); (0X10) // Read TIA control register default value
read_val[2] = LMP91000_I2CReadReg(TI_LMP91000_REFCN_REG); (0X11) // Read Reference control register default value
read_val[3] = LMP91000_I2CReadReg(TI_LMP91000_MODECN_REG); (0X12) // Read Mode control register default value
(0X01) (0X00)
LMP91000_I2CWriteReg(TI_LMP91000_LOCK_REG, TI_LMP91000_WRITE_UNLOCK); // unlock the registers for write
(0X10) (0X18)
LMP91000_I2CWriteReg(TI_LMP91000_TIACN_REG, TIACN_NEW_VALUE); // Modify TIA control register
read_val[1] = LMP91000_I2CReadReg(TI_LMP91000_TIACN_REG); // Read to confirm register is modified
(0X10)
// test if write/read values match
if (read_val[1] == TIACN_NEW_VALUE) (0X18)
{
while (1) // no error: blink LED continuously
{
__delay_cycles(250000);
__delay_cycles(250000);
TI_LMP91000_LED_PxOUT ^= TI_LMP91000_LED_PIN;
}
} else
{
TI_LMP91000_LED_PxOUT &= ~TI_LMP91000_LED_PIN; // error: Set LED OFF
}
(0X10) (0X03)
LMP91000_I2CWriteReg(TI_LMP91000_TIACN_REG, TI_LMP91000_TIACN_REG_VALUE); // store default value back in TIACN
(0X01) (0X00)
LMP91000_I2CWriteReg(TI_LMP91000_LOCK_REG, TI_LMP91000_WRITE_LOCK); // lock the registers
TI_LMP91000_MENB_PxOUT |= TI_LMP91000_MENB_PIN; // Disable \MENB Pin