你好,
我们想使用IWR6843QAGABL芯片做电路,刷机口我们连接出E14,D13,E3,E15做一个jtag接口,然后外面我们使用一个xds110调试器也连接到对应的针脚,请问这样做能否完成刷机和调试(就像使用ICBOOTS上J11口一样使用,然后还可以通过css调试)?我们在硬件的设计上还需要做其他什么么?
谢谢!
我们的调试器类似下面这样
你好,
我们想使用IWR6843QAGABL芯片做电路,刷机口我们连接出E14,D13,E3,E15做一个jtag接口,然后外面我们使用一个xds110调试器也连接到对应的针脚,请问这样做能否完成刷机和调试(就像使用ICBOOTS上J11口一样使用,然后还可以通过css调试)?我们在硬件的设计上还需要做其他什么么?
谢谢!
我们的调试器类似下面这样
user6302595 说:刷机口我们连接出E14,D13,E3,E15做一个jtag接口
芯片的jtag由专门的引脚:
TCK I JTAG Test Clock P10
TDI I JTAG Test Data Input R11
TDO O JTAG Test Data Output N13
TMS I JTAG Test Mode Signal N10
你如果手上由IWR6843ISK+MMWAVEICBOOST,你可以尝试用的仿真器廉价而MMWAVEICBOOST上的JTAG接口,并注意下面的信息:
mmWaveICBoost and Antenna Module User's Guide (SWRU546B)
2.7.5 TI 14-Pin JTAG Connector (J19)
This connector provides a JTAG interface shown in Figure 21 for debug and development through
external XDS emulators. To use this interface, the JTAG lines to the onboard emulator (XDS110) must be
disconnected and this is done with S1 (12th position of DIP switch should be open) and external emulator
on MIPI 60-pin connector also to be disconnected.
你自己板子上的JTAG接口也请参考MMWAVEICBOOST上的设计。
user6302595 说:你好,
我没有明白,开发板上只有一个232的串口连接到了6843上,但是电脑却可以看到两个uart(一个cfg,和一个data),这是怎么回事啊?
谢谢,答复。
ISK上由使用一颗MCU TM4C1294NCPDTT3 (U6)来实现了XDS110仿真器的功能,并且转换了两个串口到usb接口。原理图上你可以看到两路串口信号和JTAG相关信号都有输入到这颗MCU U6上,
你好,
报歉前面有误,是MMWAVEICBOOST上的MCU芯片。