最近用LM239A比较器做交流采样电压的阀值比较,整个采样电压系统有1.25V直流的抬升电压,LM239A的工作电压为3.3V,但是当我将比较阀值电压设置为3V时,采样过来的交流电压峰值还只到2.52V时LM239A就出现比较翻转,用示波器看了多次,采样电压没有尖峰毛刺,且采样值准确无误。一直感觉很奇怪,请群里的大神分析一下,这个是什么原因引起的?是否跟LM239A的共模电压有关系?
您好,看了下LMV339的datasheet, 2.7V供电,最大输入电压为2V,5V供电,最大输入电压4.2V,所以3.3V供电,最大也要在2.6V左右,3V是不能输入的。
4通道的您可以看下TLV3494: