drv8302在使用过程中会概率性出现内部驱动电源GVDD输出为0的情况

Other Parts Discussed in Thread: DRV8302

drv8302在使用过程中会概率性出现内部驱动电源GVDD输出为0的情况,此时使用EN_GATE引脚功能失效,对引脚拉低,拉高不能清除芯片报错以及使GVDD重新输出,但是此时测量芯片供电PVDD是正常的。只有重新给芯片的供电重新下电,上电才能使GVDD重新输出,DRV8302的外围电路是按照2011版本的数据手册上的推荐电路设计的。想请教一下出现这种情况,是哪方面的原因引起这种现象的呢?

在使用过程中,EN_GATE引脚输入信号加了RC滤波,下面是EN_GATE的波形,是否是使能信号边沿过缓导致的呢?

  • GVDD掉0的时候是有报错信号的是吗?

    EN_GATE拉低拉高10us即可清除除了GVDD_OV以外的错误。如果你确认EN_GATE不起作用,GVDD_OV可能性最大。

  • 是的,故障的时候GVDD输出为0,Nfoult报错信号一直在,使用EN_GATE,无法清除。但是EN_GATE引脚拉低20US以上不就是完全复位了吗?我在故障出现后使用的是EN_GATE的完全复位模式,拉低拉高的时间在ms级甚至s级,这样还是不能清除错误信号以及使GVDD重新输出。用示波器抓取故障时刻的GVDD以及N_FOUL波形时,GVDD并未出现过压,幅值一直是在11V左右,不过故障前,GVDD重复出现几次电压跌至欠压阈值。之后GVDD就没输出了
  • 清除的前提是故障已经不存在了,这样才能用拉低EN_GATE的方式清除保护和报错。你描述的情况看上去是故障仍然存在,需要去看一下有什么错误。比如GVDD/PVDD/AVDD几个电压,Charge Pump电压,过电流等常见错误。规格书中有列举各种故障的反应。
  • 根据规格书中的故障反应,GVDD输出为0的时,是执行了shut down charge pump 吗?如果是,那就是GVDD过压,和过温(OCTSD),过温的话可能性不大,因为现在是用两套设备在实验,两台设备的电机重复同样的动作,一台EN_GATE始终为高,这台设备上的DRV8302未出现故障,出问题的是使用EN_GATE控制电机启停的。如果是GVDD过压,那么DRV8302是检测到一次过压之后就无法恢复,只能重新给芯片上下电了吗?