DRV8832DGQR电机驱动,不能限流保护



大家好,问题是这样的:我使用DRV8832DGQR电机驱动芯片,按照规格书设计,要求是当电机堵转的时候,可以起到限流切断保护作用;然后设计的Risense阻值是0.2R,按照格式是0.2/0.2=1A限流,我电机的堵转电流是1.2A,按照理论,当我堵转电机的时候,应该起到限流保护作用,然后目前的现象是:当堵转电机,Faultn有低电平输出,但是芯片没有切断保护,还持续有0.4-0.6A的电流在工作,请问为什么还有0.4-0.6A的电流存在呢?不是直接切断变为0吗?

  • 规格书7.3.5,Current Limit只限流,报错,电机运行照旧。

    The motor current is sensed by monitoring the voltage across an external sense resistor. When the voltage exceeds a reference voltage of 200 mV for more than approximately 3 µs, the PWM duty cycle is reduced to limit the current through the motor to this value. This current limit allows for starting the motor while controlling the current. If the current limit condition persists for some time, it is likely that a fault condition has been encountered, such as the motor being run into a stop or a stalled condition. An overcurrent event must persist for approximately 275 ms before the fault is registered. After approximately 275 ms, a fault signaled to the host by driving the FAULTn signal low. Operation of the motor driver will continue.

  • 谢谢您,那么我需要堵转的时候电流截止这个功能,请问TI还有其他型号推荐吗?还有就是芯片供电电压需要达到10V,麻烦推荐个型号,谢谢了