Other Parts Discussed in Thread: DRV2700
尊敬的工程师:
您好,我在使用TI的DRV2700驱动压电驱动器,参考SLOU407A文档采用了flyback模式进行电路设计,达到500V输出没啥问题,现在我们的需求是需要达到1000V。按照芯片手册SLOS861B所述,应该可以达到1000v,我们按照计算公式调整了电阻和电容使其达能达到1000v,但是还是只有500v,所以就不知道什么原因。我们变压器还是采用的1:10,测量变压器的原边也就是SW引脚的地方,最大也只有50V,但是根据文档,SW这个引脚连接的变压器的原边可以达到100v,我们更改了电阻也不能达到,不知什么原因,谢谢!
目前lower电容4.1nF lower电阻5.502k upper电容0.022nF upper电阻4.1k
望能指教,谢谢!
祝您好心情!
Frank