i have three questions.
the first question: I have bought the MMWCAS-DSP-EVM and the MMWCAS-RF-EVM. Through the mmwave studio,I found that the data i captured was stored in the ssd and then i follow the user guide use the gui to post-processing。the range ,angle and the velocity of the object were calculated by matlab。so what is the dsp board ’s function?can i just get the range and angle and velocity through the dsp board without any applications such as matlab.
The second question:when i was testing the case3:TX Beam Forming Configuration ,there was a script Cascade_Configuration_TXBF.lua that used advanced frame configuration I can’t understand。In this script ,there is a function named ar1.AdvanceFrameConfig_mult() that I want to know its detail and these parameter’s meaning.and what ‘s the difference between frame configuration and the advanced configuration.
The third question:how to reflect the object’s range,angle and velocity timely by using the MMWCAS-DSP-EVM and the MMWCAS-RF-EVM.