Other Parts Discussed in Thread: CDCLVC1102
你好,我们在使用CDCLVC1102PWR时,发现参考设计立面在CLKIN端加了一个直流偏置电压。我在CDCLVC1102PWR的datesheet中没有发现需要加直流偏置,请问一下是否有必要添加。
请查看数据手册6.3 Recommended Operating Conditions,如下截图:
非常感谢!
我查看了一些常用的38.4MHz的晶振,貌似大部分的峰峰值都是大于0.8V。我实际量测了一个我们使用的,实际数值在1V左右。
1.是否有推荐的峰峰值大于1.2V的38.4MHz的晶振;
2.若这样的晶振不好寻找,VDD=2.3~2.7V的峰峰值要求大于1.8V即可。我可以将供电电压改成这样就可以了。