Other Parts Discussed in Thread: TMUX1112
连接上该芯片后,感觉传感器输出的电压被钳在一定范围,阅读芯片手册,并没有发现有钳位功能,是否触发了芯片的ESD二极管功能,还是该芯片内部有TVS二极管?传感器输出电压被控制的范围为4V,远低于ESD的保护电压,吹掉TMUX1112后,传感器输出电压正常,5-6V,请专家解答
您好,
我们供电电压3.3V,意思就是VS VD的输出的电压会自动在0-3.3V对吗,不会超过3.3V,相当于内部有个二极管,把输出电压就控制在了3.3V以内?我们传感器的一脚就是直接和VS or VD连接的。您后边指的请注意信号范围,是在提醒会损坏片子的意思吗?我们传感器负端与TMUX1112芯片的开关3连接,我测试的是示波器一端接传感器负,一端接板子的地,而且测试的时候,TMUX1112芯片使能脚是低电位,只有3.3V供电,开关处于断开状态,不存在压降降在了电阻上。