Other Parts Discussed in Thread: TMUX1112
The valid signal path input/output voltage for TMUX111x ranges from GND to VDD. 这句的意思是不是说,通过开关后的输出最大就是VDD,但是会影响输入信号吗。我的理解是,在不考虑损坏片子的基础上,输入有多大就应该是多大,然后输出会被钳位在VDD,假如VDD是5V,开关的输入是8V,然后测试输出一端应该就是5V,这个理解对吗?关于轨对轨的理解,烦请专家多解释解释。
还有1个问题,假如,我们的激励信号接芯片的S1脚,我们传感器的正端,接芯片的D1脚,传感器的负端接S2脚,D2脚接地的方式,通过开关1控制激励信号是否加载至传感器中,通过开关2保证传感器与地隔离。用示波器测试传感器负端对地电压,正常可达5-6V(不接TMUX1112芯片),片子是3.3V供电的,按照上述方式连接的话,传感器负端对地电压一直为4V左右(连接片子),低于正常值,感觉TMUX1112芯片起到了钳位器的作用,传感器的输出电压不控制在了4V以下,不知道这个现象是不是和上边轨对轨有关系。测试过程中,TMUX1112芯片只是3.3V供电,开关均处于断开的状态,应该不存在开关电阻分压的情况。
前几天问过1次此类问题,解答了以后,直接跟帖再回复就可以了吗?跟帖回复了以后,我看没专家接着回复了,才发了1个这次的新帖。