可以用AWR1642来进行官方示例的生命体征检测实验吗?

Other Parts Discussed in Thread: AWR1642, AWR1642BOOST-ODS, AWR1642BOOST

官方有生命体征实验,但只有用14xx的源代码。官方提供的项目可以直接用在AWR1642上吗?

  • 图片显示不出来,请点击"回复"后,点击右下角的“使用高级编辑器编辑文本”插入图片,谢谢!
  • Resource Explorer 中Vital Signs里只有14xx和68xx的,可以用AWR1642来运行这个实验吗?需要改动什么地方吗?

  • Resource Explorer 中Vital Signs里只有14xx和68xx的,可以用AWR1642来运行这个实验吗?需要改动什么地方吗?

  • 请参考automotive toolbox 2.9.1里有Driver Vital Signs
    dev.ti.com/.../node

    另外,可以看一下下面的培训视频。
    training.ti.com/.../driver-vital-sign-detection-demonstration-using-mmwave-radar-sensors
  • 你好,按照Getting Started Guide到最后一步打开VitalSignsRadar_Demo.exe弹出GUI界面并点击Start后就没有反应了,也没有出来波形什么的,下面是黑框里的显示,应该是连接上板子了,请问这要怎么解决呀?

    另我用的是AWR1642BOOST-ODS这有影响吗?

    QT version = 5.9.1
    QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted()
    Serial Port Found
    Data Port Number is "COM7"
    User Port Number is "COM8"
    Data port succesfully Open
    User port succesfully Open
    QWindowsWindow::setGeometry: Unable to set geometry 1485x999+8+31 on QWidgetWindow/'MainWindowWindow'. Resulting geometry: 1370x749+8+31 (frame: 8, 31, 8, 8, custom margin: 0, 0, 0, 0, minimum size: 1347x749, maximum size: 16777215x16777215).
    Configuration File Name Read from the GUI is %s/n "xwr1642_profile_VitalSigns_20fps_Back.cfg"
    QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted()
    "COM8"
    Configuration File Path is %s/n "D:/Program Files/ti/ccs930/mmwave_automotive_toolbox_2_9_1/labs/lab0001-driver-vital-signs/vitalSigns_host/profiles/xwr1642_profile_VitalSigns_20fps_Front.cfg"
    "sensorStop"
    "flushCfg"
    "dfeDataOutputMode 1"
    "channelCfg 15 3 0"
    "adcCfg 2 1"
    "adcbufCfg -1 0 0 1 0"
    "profileCfg 0 77 7 6 57 0 0 70 1 200 4000 0 0 48"
    "chirpCfg 0 0 0 0 0 0 0 1"
    "frameCfg 0 0 2 0 50 1 0"
    "lowPower 0 1"
    "guiMonitor 0 0 0 0 1"
    "calibDcRangeSig -1 0 0 0 0"
    "vitalSignsCfg 0.3 0.9 256 512 4 0.1 0.05 100000 300000"
    "motionDetection 1 20 2.0 0"
    "sensorStart"
    ""
    "sensorStop"
    "flushCfg"
    "dfeDataOutputMode 1"
    "channelCfg 15 3 0"
    "adcCfg 2 1"
    "adcbufCfg -1 0 0 1 0"
    "profileCfg 0 77 7 6 57 0 0 70 1 200 4000 0 0 48"
    "chirpCfg 0 0 0 0 0 0 0 1"
    "frameCfg 0 0 2 0 50 1 0"
    "lowPower 0 1"
    "guiMonitor 0 0 0 0 1"
    "calibDcRangeSig -1 0 0 0 0"
    "vitalSignsCfg 0.3 0.9 256 512 4 0.1 0.05 100000 300000"
    0.3
    0.9
    4
    "motionDetection 1 20 2.0 0"
    "sensorStart"
    ""
    Chirp Duration in us is : 50
    Chirp Bandwidth in kHz is : 3500
    Maximum Range in Meters is : 8.57143
    Range-FFT size is : 256
    Range-Bin size is : 0.0334821
    Range-Bin Start Index is : 8
    Range-Bin End Index is : 26
    Total Payload size from the UART is : 260
    Padding Factor is : 9
    Total Payload size from the UART is : 288

  • 这个demo只支持AWR1642BOOST ES 2.0 EVM。
  • 那请问有适配AWR1642BOOST-ODS的吗?