AWR2243 LVDS信号读取问题

Other Parts Discussed in Thread: DCA1000EVM, SN65LVDT348, AWR2243

你好!

我们目前使用外部MCU通过SPI对AWR2243BOOSTEVM进行配置;计划使用SN65LVDT348差分转单端芯片对LVDS信号进行转换,再通过FPGA接收。

模块使用DCA1000EVM+mmwave studio进行控制和采集时一切正常。在使用外部MCU时我们参考了AWR2243-Interface-Control.pdf与mmwave_dfp_user_guide.pdf,已经可以对模块进行参数配置和启停控制。

在测试LVDS波形时发现波形异常,我们将7个LVDS通道接入差分转单端芯片,然后测量其差分端的波形:VALID和FRCLK通道的偏置电压为2V,CH0~CH3及BITCLK通道的偏置电压为0.7V,同时所有通道的振幅都只有20~30mv。显然不是LVDS工作的正常范围。SN65LVDT348芯片内置100欧匹配电阻,外围电路经查无误。

请问:1.AWR2243是否有相关配置会影响到LVDS输出,从而出现上述现象?

2.直接通过LVDS转换芯片读取的方法是否可行,是否需要在软硬件上进行额外配置?