Other Parts Discussed in Thread: AWR2243
- 该雷达对人的最大探测距离
- 9-TX模式的配置参数(如何配置)
- maging Radar Using Cascaded mmWave Sensor Reference Design这个文档里4.2.3.2和4.2.3.3这两个试验对应的雷达配置参数
Other Parts Discussed in Thread: AWR2243
该雷达对人的最大探测距离
你可以在下面的文档找到相关信息:

4.2.3.2 Pedestrian Long-Range Detection
In this test a pedestrian jogging from 30 m to 140 m. The AWR2243 Cascade RF board is running in 9-TX
beamforming mode.
The range profile shows the pedestrian at 120 m with 20-dB SNR. The Doppler-Range plot is shown to
the right. Slight Doppler displacement can be seen corresponding to the pedestrian velocity.
你可以参考C:\ti\mmwave_studio_03_00_00_14\docs\mmwave_studio_cascade_user_guide.pdf, C:\ti\mmwave_studio_03_00_00_14\mmWaveStudio\MatlabExamples