Other Parts Discussed in Thread: TMUX136
1、单级tmux136芯片和三级tmux136芯片在使用中能达到的带宽相差多大,还是带宽不受芯片多级联影响。
2、规格书中写的带宽(-3dB):6.1GHz,Bandwidth曲线图中也显示带宽在1G以内时都是dB(S(2,1))>-0.5,1G以内的频响很好基本上是一条直线,但是我们实测发现不是的,在100MHz时就出现了dB(S(2,1))<-1.5的情况,是不是-3dB在1GHz带宽范围内也是周期出现的。
3、如果可以达到,多级联芯片设计时需要注意什么,带宽才能达到规格书Bandwidth曲线图中显示的带宽在1G以内时都是dB(S(2,1))>-0.5,1G以内的频响是一条近似直线。
4、你们测试带宽是不是使用的常用的测试方法,如果不是常用的你们使用的是什么测试方法。