请问一下,我将LMP91000的MODECN寄存器设置为1000 0011,之后是否直接连接三引脚气体传感器即可?为什么我的VOUT端的电压始终是5V?是否需要设置其他的寄存器?
你好,你可以参考一下MSP430 Interface to LMP91000 and LMP91002 Code Library, snac032.zip,在产品主页上软件那一栏
如果需要配置成3极电池测定模式,需要将MODECN配成0x03,0X02是配置成standby模式,也是一种省电模式,并不是测量气体浓度模式,你可以参考datasheet 中 Table3的各种模式下的功耗。
测量气体浓度的时候应该把寄存器配置成0x01,并且有关浓度的,有一个计算公式:
Gas sensitivity (nA/ppm) X Gas concentration (ppm) = Sensor Output Current (nA).