如上图所示:系统设计要求为利用锁相环CD4046相位比较器Ⅱ进行二倍频,输入频率信号范围为1~200Hz的低频信号,希望输出得到2~400Hz的信号。
测试表明实验结果满足要求,但是遇到一个问题,此电路会增加系统电源的噪声。本系统是采用12V电池供电,通过TPS7A4901转换成5V给CD4046供电。此电路工作时5V电源上(即电路中的A点)会有一个和CD4046工作频率相同的噪声信号,但是幅度比较小,只有几mVp-p。如下图所示
但是此噪声会折返到12V电源上(即电路中的B点),噪声频率依然和CD4046工作频率相同,而且幅度很大,达到70多mVp-p。如下图所示
尝试改变不同的频率发现5V电源上(B点)的噪声频率始终和CD4046工作频率相同,且幅度一直都是4mVp-p左右。
但是折返到12V电源上(A点)的噪声会随着工作频率的增大而变小,频率始终和CD4046工作频率相同。下面的图是不同工作频率时12V电源(A点)的噪声情况及波形。如下面的图示
当工作频率为10Hz时12V电源上的噪声高达100mVp-p,随着工作频率的增加,噪声逐渐减小,当工作频率为1KHz时12V电源上的噪声为37mVp-p。由于12V电源还要给系统的其他部分供电,所以有很大影响。不知道是什么原因造成的,希望TI工程师能给予解决方案。