Other Parts Discussed in Thread: DRV8837
IN1输入PWM(VCC高3.3V),IN2输入高电平,OUT1输出低电平,OUT2输出PWM(VM高5V)
IN2输入PWM(VCC高3.3V),IN1输入高电平,OUT2输出低电平,OUT1输出PWM(VM高5V)
PWM通过调占空比控制电压大小,用8837就是想改变方向,两个方向都能输出,并且将电压VCC提高到VM。
1、这样设计的电路有问题么?
2、我试了三块芯片,两个没有问题,都能正常输出,但是有一个不知道怎么了,只能输出一个方向,IN1和IN2改变输入,OUT不能跟着改变。是我这样输入导致芯片烧坏了么?
3、DRV8837芯片可以同时输入高电平么?使用这款芯片时需要注意什么?
4、是不是我接的负载是感性元件线圈,反电动势烧坏了芯片?对于感性元件线圈,需要注意些什么?怎么消除反电动势?DRV8837是否可以消除反电动势?
5、DRV8837输入PWM频率范围是多少?
6、有必要在输出端加低通滤波电路么?
求指教。多谢。