Other Parts Discussed in Thread: LM1875, L293D
就是希望在恒流源提供电流,负载为电阻,电压为40V左右提供的情况下用单片机控制,可以达到这样一个波形效果,峰值不需要平稳,不需要连续,只是间断的这样的一个个波,其实就相当于接一个H桥,负载为一个电阻,我是考虑使用控制步进电机的芯片来达到这样效果,想问下什么芯片额可以达到这种效果?使用步进电机的芯片是否可行?
L293D电压范围不满足,可以看看SN75476。你能不能在详细说一下输入和输出信号?
您好,
系统是否需要产生一个40V的电压? 0.1A的电流,使用分立器件也是可以的。