在datasheet第5页中,我看到VB有三个参数VB1 VB2 VB3 ,那么问题来了,DRV3203可以应用在24V汽车供电系统么?
另外 如果还有迷惑请参考如下信息:
VB1 : This is for which Electrical char is guaranteed. Please ignore disregard (motor operation).
VB2 : This is inteded for min only. No RESET until VB<4.5. Max=18v does not mean anything.
VB3 : 18v-26.5v Functionality is guaranteed. Electrical char is guaranteed by design. Basically device works upto min of VB over voltage.
Lastly VB abs max is 40v since it is for auto.
应该不需要俺给你翻译吧,呵呵