专家你好,我购买的ADS1298芯片参照datasheet第80面及81面画PCB板制板后,用Arduino做处理器操作芯片,但是示波器检测不到DOUT有任何变化。芯片不工作,目前我用的是单极型接法。恳请答复。
代码如下:
#include<SPI.h>
void setup() {
// put your setup code here, to run once:
Serial.begin(9600);
SPI.begin(4);
SPI.setBitOrder(4,MSBFIRST);
SPI.setDataMode(4,SPI_MODE1);
SPI.setClockDivider(4,42);
//SPI.transfer(4,0xFF,SPI_CONTINUE);
}
void loop() {
// put your main code here, to run repeatedly:
// delay(1000);
SPI.transfer(4,0x20,SPI_CONTINUE);
SPI.transfer(4,0x02,SPI_CONTINUE);
unsigned char ret=SPI.transfer(4,0x01);
Serial.write(ret);
}