目前设备:TDC1000-GASEVM + HV board 、 win7PC、 1MHz传感器、水杯(传感器穿过水杯相对安装)。
目标:测静态水流量。
一、连接EVM与PC后,GUI显示 Read ALL No Errors,
On the TDC1000-GASEVM, make sure the following jumpers are in place.
1. JP1: TDC7200 - connect pin 1 to pin 2 (via a jumper)
2. JP2: CPU - connect pin 1 to pin 2 (via a jumper)
3. JP3: TDC1000 - connect pin 1 to pin 2
4. JP4: VIO - connect pin 1 to pin 2
5. JP5: Trigger - connect pin 2 to pin 3
6. JP6: CLOCK - connect pin 5 to pin 6 这里我使用的是 OSC 不是5-6的CPU时钟
二、连接示波器探针到:TX1、START。但EVM未连接传感器。
三、 select the "TDC1000-HV Driver EN1", 然后在GRAPH页面,按 START GRAPH。
上述操作后 GUI提示 reading Graph data 成功,但绘画无显示,TEMP AVG 框内:0.0.0(degc). 示波器上面没有激励波形出现。
我的操作有什么问题,导制EVM没有激励波形输出,按猜测不接上传感器也能在TX1端看到激励波形。