lmp91000 寄存器LOCK -- Protection Register (Address 0x01)锁定



The lock bit enables and disables the writing of the TIACN and the REFCN registers. In order to change the
content of the TIACN and the REFCN registers the lock bit needs to be set to “0”.

Bit                                      Name                                                        Function
[7:1]                                  RESERVED                                   Write protection
                                                                                                    0   LOCK 0 Registers 0x10, 0x11 in write mode
    0                                        LOCK                                            1    Registers 0x10, 0x11 in read only mode (default)

TIACN  REFCN 寄存器配置好了,然后锁定好。断电,再上电 TIACN  REFCN 上次配置的值还在不啊???