Other Parts Discussed in Thread: LM3S8962
我是使用固件库写的,编译没问题,就是下进板子不运行?不知道什么原因请大家帮忙看看是错误在哪?库函数我已经放进工程里了;
#include "pbdata.h"
void RCC_Configuration(void);
void GPIO_Configuration(void);
//#include "lm3s8962.h"
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Blinky (blinky)</h1>
//!
//! A very simple example that blinks the on-board LED.
//
//*****************************************************************************
//*****************************************************************************
//
// Blink the on-board LED.
//
//*****************************************************************************
int main(void)
{
// RCC_Configuration();
// GPIO_Configuration();
while(1)
{
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_4, 0x00);
SysCtlDelay(1000 * (SysCtlClockGet() / 3000));//1000????
//10???? SysCtlDelay(10 * (SysCtlClockGet() / 3000000))
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_4, 0xff);
SysCtlDelay(1000 * (SysCtlClockGet() / 3000));
}
}
void RCC_Configuration(void)
{
SysCtlClockSet(SYSCTL_SYSDIV_4|SYSCTL_USE_PLL
|SYSCTL_OSC_MAIN
|SYSCTL_XTAL_8MHZ);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
}
void GPIO_Configuration(void)
{
GPIODirModeSet(GPIO_PORTA_BASE, GPIO_PIN_4, GPIO_DIR_MODE_IN);
GPIOPadConfigSet(GPIO_PORTA_BASE,
GPIO_PIN_4,
GPIO_STRENGTH_4MA,
GPIO_PIN_TYPE_STD);
}