TMS320F28335PGFA中的ADC通道中的一个通道会影响其他通道的数据采集



其中我的底板上有一路六选一的多通道模拟片选电路,六路模拟信号通过片选芯片,只有一路输出,输入到ADC模块的B通道的B7。同是有另外一路模拟通道输入B6,该信号唯一固定的。六选一的模拟信号通过片选芯片循环片选时,B7通道的数据循环变化。这样会影响B通道的B6通道数据变化为零的跳动,其他几路B0~B5也不稳定。但是不会影响到A通道的数据采集。请问这是由什么原因造成的?是28335内部ADC问题吗??