LM3S5B91 PB7无法输出高电平,仿真时,寄存器是有变化的,但输出的电平始终是低电平。
B7默认为NMI特殊功能管脚,要想配置为普通IO口需要特殊操作,数据手册里有说明
//
// Convert the PB7/NMI pin into a GPIO pin. This requires the use of the
// GPIO lock since changing the state of the pin is otherwise disabled.
//
HWREG(GPIO_PORTB_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY_DD;
HWREG(GPIO_PORTB_BASE + GPIO_O_CR) = 0x80;
//
// Make PB7 an output.
//
GPIODirModeSet(GPIO_PORTB_BASE, GPIO_PIN_7, GPIO_DIR_MODE_OUT);
GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_7, GPIO_STRENGTH_8MA,
GPIO_PIN_TYPE_STD);
//
// Clear the commit register, effectively locking access to registers
// controlling the PB7 configuration.
//
HWREG(GPIO_PORTB_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY_DD;
HWREG(GPIO_PORTB_BASE + GPIO_O_CR) = 0x00;