AM335X Sitara McAsp 模块是否支持entire McASP module reset by Power and Sleep Controller(PSC)?



当前使用McAsp的通道进行数据传输,用的是Burst Mode 外加DMA试来获取数据。由于调试遇到一个问题,需要将整个McASP module进行reset.

根据手册22.2.11.1 Software Reset Considerations中提到的,
"The entire McASP module also be reset through the Power and Sleep Controller(PSC). Note that from the McASP perspective, this reset appears as a hardware reset to the entire module."根据这个提示,能够通过PSC去控制module被reset. 但从手册中PRCM章节的Power Management 中没有查到能够只将McASP module重置的register.

请问大神,帮助解释下,谢谢~