[DRA829]Question about pinmux config



Hi,

The pinmuxConfig function is a port initialize function and I think it only opearte the CTRL_MMR and MCU_CTRL_MMR registers,right?

But I think when we use the GPIO0_127 pin,we also need config the GPIO_DIR67 and GPIO_SET_DATA67 registers to set the output direction and initial level.

So is there have a function to config the GPIO direction and initial level?

Thinks,

Regards,

Linda Xie