LM4F120开发板的PWM输出问题

想使用定时器的PWM模式功能,但是发现开启了PWM模式后,定时器超时中断无法进入了,这是什么原因呢,pwm输出已经可以了,代码如下

//*****************************************************************************
//
// project0.c - Example to demonstrate minimal StellarisWare setup
//
// Copyright (c) 2012 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 9453 of the EK-LM4F120XL Firmware Package.
//
//*****************************************************************************

#include "inc/hw_ints.h"
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/timer.h"
#include "driverlib/rom.h"
#include "driverlib/interrupt.h"


//*****************************************************************************
//
// Define pin to LED color mapping.
//
//*****************************************************************************

#define RED_LED GPIO_PIN_1
#define BLUE_LED GPIO_PIN_2
#define GREEN_LED GPIO_PIN_3

//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Project Zero (project0)</h1>
//!
//! This example demonstrates the use of StellarisWare to setup the clocks
//! and toggle GPIO pins to make the LED's blink. This is a good place to
//! start understanding your launchpad and the tools that can be used to
//! program it. See http://www.ti.com/stellaris-launchpad/project0 for more
//! information and tutorial videos.
//!
//
//*****************************************************************************
unsigned long clockfre;
unsigned char bit;
void Timer0IntHandler(void)
{
ROM_TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
ROM_TimerMatchSet(TIMER0_BASE, TIMER_A, 1000);
}
//*****************************************************************************
//
// Main 'C' Language entry point. Toggle an LED using StellarisWare.
// See www.ti.com/stellaris-launchpad/project0 for more information and
// tutorial videos.
//
//*****************************************************************************
int
main(void)
{
ROM_FPULazyStackingEnable();
//设置系统频率为80Mhz
ROM_SysCtlClockSet(SYSCTL_SYSDIV_2_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|
SYSCTL_OSC_MAIN);

//使能定时器0 32/16bit时钟模块
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
//设置Timer0-A模块为PWM输出模式
ROM_TimerConfigure(TIMER0_BASE, TIMER_CFG_SPLIT_PAIR |TIMER_CFG_A_PWM);
//读取系统频率
clockfre=ROM_SysCtlClockGet();
// 设置定时器的计数值,10khz
ROM_TimerLoadSet(TIMER0_BASE, TIMER_A, 8000);
ROM_TimerMatchSet(TIMER0_BASE, TIMER_A, 6000);
// 启用系统总中断开关
ROM_IntMasterEnable();
// 在系统层面(NVIC)使能Timer0-A中断
ROM_IntEnable(INT_TIMER0A);
//使能定时器0,定时器A超时中断
ROM_TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);

GPIOPinConfigure(GPIO_PB6_T0CCP0);

ROM_GPIOPinTypePWM(GPIO_PORTB_BASE, GPIO_PIN_6);

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);

ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_2 | GPIO_PIN_1);
//使能定时器0,定时器A
ROM_TimerEnable(TIMER0_BASE, TIMER_A);

while(1)
{

}
}

  • timer 的PWM模式下不支持TIMEOUT中断,这个在datasheet中的11.3.2.5 PWM Mode章节有详述:

    The timer is capable of generating interrupts based on three types of events: rising edge, falling edge, or both. The event is configured by the TnEVENT
    field of the GPTMCTL register, and the interrupt is enabled by setting the TnPWMIE bit in the GPTMTnMR register. When the event occurs, the CnERIS bit is set in the GPTM Raw Interrupt Status (GPTMRIS) register, and holds it until it is cleared by writing the GPTM Interrupt Clear (GPTMICR) register .