LM3S9B92芯片被锁了,怎么解锁?

您好,我目前在使用LM3S9B92评估板,之前用IAR EWARM 5.4软件给板子下载了多个程序都可以正常显示,但是现在在下载编译程序的时候出现了这样的错误“fatal error:There were warnings during download of FLASH loader,see Log Window Session aborted!”,上网查了下说是开发板被锁了,我之前有取下JP55、56、57的短路帽,是不是这个原因导致的,可是重新安装好短路帽后,显示屏还是白屏什么程序都下载不进去,这是怎么回事?该怎么解决呢?非常感谢啦!

  • 如果是B1版的芯片,解锁流程如下:

    1.2 The Recover Locked Device sequence does not work as expected
    Description:
    If software configures any of the JTAG/SWD pins as GPIO or loses the ability to communicate with
    the debugger, there is a debug sequence that can be used to recover the microcontroller, called
    the Recover Locked Device sequence. After reconfiguring the JTAG/SWD pins, using the Recover
    Locked Device sequence does not recover the device.
    Workaround:
    To get the device unlocked, follow these steps:
    1. Power cycle the board and run the debug port unlock procedure in LM Flash Programmer. DO
    NOT power cycle when LM Flash Programmer tells you to.
    2. Go to the Flash Utilities tab in LM Flash Programmer and do a mass erase operation (check
    "Entire Flash" and then click the Erase button). This erase appears to have failed, but that is
    ok.
    3. Power cycle the board.
    4. Go to the Flash Utilities tab in LM Flash Programmer and do another mass erase operation
    (check "Entire Flash" and then click the Erase button).
    Silicon Revision Affected:
    B1
    Fixed:
    Fixed in Rev C.

  • 您好,请问什么是B1版本的?不好意思,初次接触不是很会,使用的是深圳大学联合实验室的,板子上面标注有DK-LM3S9B92 SZU-TI DSPS Technology Center,非常感谢!

  • 如果是有LUMINARY MICRO 的标记应该是, 应是在丝印的第二行后3和4个字母

  • 你好,我从老师那里得到一块和你一样的板子,但是没有资料。网上也没找到,官网关于这块板的资料貌似也没有。可不可以分享一下你那个评估板附带的光盘或其他资料 ,麻烦你了

  • 要不你给我你的QQ邮箱,我发到你邮箱!网速比较慢。。。

  • 你好,C1版的芯片是不是不能解锁?我对C1芯片进行解锁后,板子能下程序了,但是无法显示,好像是在解锁的过程中把C1 补丁存储区域给擦除了。这样芯片是不是就坏了,那我的DK—LM3S9B96开发板是不是只要换一块C1版的芯片就行,还是说整块板子都没用了?