stellaris,LM3S9B96的ADC问题



ADC的问题,不知道是不是9B96的问题还是我程序的问题。

void adc1Init(void)
{
// SysCtlPeripheralEnable(GPIO_PORTB_BASE);
//GPIOPinTypeADC(GPIO_PORTB_BASE,GPIO_PIN_4 );


ADCSequenceDisable(ADC1_BASE,3); // 配置前先禁止采样序列
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC1); // 使能ADC模块
SysCtlADCSpeedSet(SYSCTL_ADCSPEED_1MSPS); // 设置ADC采样速率

// 采样序列配置:ADC基址,采样序列编号,触发事件,采样优先级
ADCSequenceConfigure(ADC1_BASE, 0, ADC_TRIGGER_PROCESSOR, 1);
// 采样步进设置:ADC基址,采样序列编号,步值,通道设置
ADCSequenceStepConfigure(ADC1_BASE, 3, 0, ADC_CTL_TS |
ADC_CTL_END |
ADC_CTL_IE ) ;
ADCReferenceSet(ADC1_BASE,ADC_REF_INT);
ADCResolutionSet(ADC1_BASE,ADC_RES_10BIT) ;
ADCIntClear(ADC1_BASE, 3);
ADCSequenceEnable(ADC1_BASE, 3); // 使能采样序列
ADCIntEnable(ADC1_BASE, 3); // 使能ADC中断
IntEnable(INT_ADC1SS3) ; // 使能ADC采样序列中断
IntMasterEnable() ; // 使能处理器中断

}

在DKLM3S9B96上跑的。换ADC0就能工作,换ADC1就不能工作。调用这个初始化函数,程序就会死在里面。何解?中断向量也注册了

  • 参考例程如下:


    //*****************************************************************************

    #include "inc/hw_ints.h"
    #include "inc/hw_memmap.h"
    #include "inc/hw_types.h"
    #include "driverlib/gpio.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/adc.h"
    #include "driverlib/timer.h"
    #include "utils/ustdlib.h"
    #include "utils/uartstdio.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/systick.h"
    #include "utils/cmdline.h"


    void Delay(unsigned long count )
    {
    unsigned i,j;
    for(i=0;i<count;i++)
    {for(j=0;j<count;j++) ; }
    }


    int iADC0_read=1;                // Indicates if the ADC is ready (1) or busy (0)
    unsigned long ulBlinkSpeed = 0;  // Timer interrupt frequency (0=low; 1=high)
    //************ User Defines ************
    //
    // 12-bit resolution bit
    //
    //#define ADC_RES_12BIT 0x10

    //
    // Offset for ADC control register
    //
    #define ADC_O_CTL 0x38

    //*****************************************************************************
    // Interrupt handler for the Timer0 interrupt
    //*****************************************************************************
    void Timer0IntHandler(void)
    {
        unsigned long ulPinStatus;
       
        // Clear the timer interrupt.
        TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);   

        // Read the current state of the output
        ulPinStatus = GPIOPinRead(GPIO_PORTD_BASE, GPIO_PIN_0);
       
        // Toggle Bit 0
        ulPinStatus ^= GPIO_PIN_0;
       
        // Write the result back into the GPIO Pin 0 Data Register
        GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_0, ulPinStatus);

        // Check if the ADC is ready
        if (iADC0_read == 1)
        {
            // Trigger new ADC Conversion using Sample Sequencer 0
            ADCProcessorTrigger(ADC1_BASE,2);
           
            // Indicate that the ADC is busy
            iADC0_read = 0;
        }
    }

    //*****************************************************************************
    // Interrupt handler for the ADC Sample Sequencer 2 (SS2) interrupt
    //*****************************************************************************
    void ADC2IntHandler(void)
    {
        unsigned long adc0Value[4]={0,0,0,0};   // Holds the ADC result
        char adc0String[4];        // Holds the string-converted ADC result
     unsigned long InputVoltage; //Input voltage
        // Clear the ADC0 interrupt.
        ADCIntClear(ADC1_BASE,2);
       
        // Read the data from the Result Buffer of ADC SS2
        // We know that we have only one result in the buffer
        // If we have more than one result then adc0_value must be an array
        ADCSequenceDataGet(ADC1_BASE, 2,adc0Value);
     
     //ADC AT 12 BIT MODE,PLEASE REFER TO ADC CONVERSION VALUE Y=1352X+28 =>INPUT VOLTAGE VALUE X=((Y-28)/1352)*1000(MV)
         InputVoltage= (adc0Value[0]-28/1352)*1000;
     // Delay(6553000);
        //adc0Value[1]=((1475 * 1023) - (2250 * adc0Value[1])) / 10230;   //centigrade temperature


        IntMasterDisable();
        UARTprintf("\n%d",adc0Value[0]);
        UARTprintf("\n%d",adc0Value[1]);

        //UARTprintf("\n%d",adc0Value[2]);
        //UARTprintf("\n%d",adc0Value[3]);
     
     
      
        // Disable interrupts globally to ensure we don't interrupt communication with the display
        //IntMasterDisable();
      
        iADC0_read = 1;   
       // while(1);
        // Re-enable interrupts globally
        IntMasterEnable();
    }


    int main(void)
    {

        //*****************************************************************************
        // Clock Setup
        //***************************************************************************** 
     
        // Set the clocking to run directly from the crystal.
        SysCtlClockSet(SYSCTL_SYSDIV_4| SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);

      
       
        // Enable Timer 0, ADC0 and GPIO Block D Peripheral Clocks
        SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC1);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
      
       //LED on PD0
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
      // Reset the state of Peripheral ADC0
        //
        //SysCtlPeripheralReset(SYSCTL_PERIPH_ADC0); 
     
     //
     // Setup the AIN0 on PE7 ...
     //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);

        GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3);
        //GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_6);
        //GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_5);
       // GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_4);

        // Enable the peripherals used by this example.
        //

     

     
       IntMasterDisable();
        //
        // Set GPIO A0 and A1 as UART.
        //
        GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

        //
        // Initialize the UART as a console for text I/O.
        //
        UARTStdioInit(0);

        //
        // Print hello message to user.
        //
        UARTprintf("\n\nADC Test Example Program\n");
       


        //*****************************************************************************
        // GPIO Setup
        //*****************************************************************************     
       
        // Set GPIO_F, pin 0 as output (used for the LED)
        GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_0);
       
        // Disable processor interrupts
        IntMasterDisable();
       
        //*****************************************************************************
        // Timer 0 Setup
        //***************************************************************************** 
       
        // Configure Timer0 as 32-bit periodic timer   
        TimerConfigure(TIMER0_BASE, TIMER_CFG_32_BIT_PER);
       
        // Set Timer0 period as 1/4 of the system clock, i.e. 4 interrupts per second
        TimerLoadSet(TIMER0_BASE, TIMER_A, SysCtlClockGet() /4);

        // Configure the timer to generate an interrupt on time-out
        TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);   
       
        // Enable the TImer Interrupt in the NVIC
        IntEnable(INT_TIMER0A);

        // Enable the timer                   
        TimerEnable(TIMER0_BASE, TIMER_A);
     
        //
     // Set 12-bit resolution
     //
       HWREG(ADC1_BASE + ADC_O_CTL) = HWREG(ADC1_BASE + ADC_O_CTL)| ADC_RES_12BIT;

     //
     
        ADCSequenceConfigure(ADC1_BASE,2, ADC_TRIGGER_PROCESSOR, 0);

        ADCHardwareOversampleConfigure(ADC1_BASE,16);
     
        ADCSequenceStepConfigure(ADC1_BASE, 2,0, ADC_CTL_CH0);      //ADC0 channel 0

       ADCSequenceStepConfigure(ADC1_BASE, 2,1, ADC_CTL_TS|ADC_CTL_IE | ADC_CTL_END );  //setup temperature channel

     
         // Clear the ADC0 interrupt.
        ADCIntClear(ADC1_BASE,2);
     
        ADCIntEnable(ADC1_BASE, 2);

     
        // Enable ADC SS2
        ADCSequenceEnable(ADC1_BASE, 2);

     

     // Enable the ADC0 interrupt in the NVIC
        IntEnable(INT_ADC1SS2);
       
       
        // Indicate that ADC SS2 is ready for sampling
        iADC0_read = 1;   

        //*****************************************************************************
        // Global Interrupt Enable
        //***************************************************************************** 
       
        // Enable processor interrupts
        IntMasterEnable();
        IntPrioritySet(INT_TIMER0A,0x40);
        IntPrioritySet(INT_ADC1SS2,0x40);
        // Loop forever waiting for interrupts

     

        while(1)
        {
        }
    }