Other Parts Discussed in Thread: TRF7960, LM3S811, TRF7970A
我的硬件电路参考TI的设计【Stellaris 13.56 MHz RFID 无线套件的主要特性与优势 (DK-EM2-7960R)
】,
【问题1】现在,我的天线可以在2厘米以内寻到Mifare 1的卡UID,但是认证没有通过,或偶尔可以认证成功,频率极低,即,在 文件中执行函数,
int
MIFAREOpen(unsigned int uiKeySelect, unsigned int uiBlock,
unsigned char const *pucKey, unsigned int uiKeySize,
unsigned char *pucUID, unsigned long *puiUIDSize, int iCard)
到
iRes = MIFAREAuthenticate(uiKeySelect, uiBlock, pucKey, uiKeySize,
pucUIDTmp, uiUIDTmpSize);
在iRes = MIFAREAuth1(uiKeySelect, uiBlock, pucUID, uiUIDSize);返回认真错误。
但是,这个例程我在开发板上实验是可以的。是不是认真M1需要特殊的文件?TRF7960的评估板上有一个EEPROM,这里面存储操作TRF7960的信息吗?
【问题2】我用LM3s811控制TRF7960,所有外设和天线都在一个板上,我用JTAG调试时很难寻到卡片并且距离很近必须要贴近天线板,但是我不插JTAG调试器,全速运行时只要卡片接近天线就马上被发现,这是什么原因?
【问题3】这是我第一次做射频的东西,对天线调制还不是很了解,我感觉还是天线调的不好,我想知道在现在调试已经做成PCB的天线,用实验的方式怎么调?