Other Parts Discussed in Thread: LM3S6911
这个型号是什么时候出来的?感觉是6911的主频和FLASH升级版,引脚和6911也是兼容的。有几个问题麻烦解答:
1、BOOTLOADER:如果是批量生产,是不是可以去掉板子上的JTAG口?新器件可以直接从以太网端口烧程序吗?(ROM中的BOOTLOADER已经默认使能Ethernet了吗?6911要先烧个以太网配置的BOOTLOADER代码才行)。
2、发热量和6911相比有改进么?
3、调用ROM中的驱动或者调用FLASH里面的驱动,不考虑空间的话哪个好?
4、有两个UART同时独立工作,波特率和收发数据量都很高(1.5Mbps),在6911上用FIFO的RX/RT中断处理不过来。用DMA方式收发数据是否可以提高性能?
5、从6C11转到6911还要注意哪些?
6、有没有6C11的评估板?
非常感谢!