unsigned int i;
signed int j1=0,j0=0;
//
// The FPU should be enabled because some compilers will use floating-
// point registers, even for non-floating-point code. If the FPU is not
// enabled this will cause a fault. This also ensures that floating-
// point operations could be added to this application and would work
// correctly and use the hardware floating-point unit. Finally, lazy
// stacking is enabled for interrupt handlers. This allows floating-
// point instructions to be used within interrupt handlers, but at the
// expense of extra stack usage.
//
//FPUEnable();
//FPULazyStackingEnable();
//
// Set the clocking to run directly from the crystal.
//
SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |SYSCTL_XTAL_6MHZ);//80MHZ
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_QEI1);
ROM_GPIOPinTypeQEI(GPIO_PORTC_BASE,GPIO_PIN_5);
ROM_GPIOPinTypeQEI(GPIO_PORTG_BASE,GPIO_PIN_4);
ROM_QEIConfigure(QEI1_BASE,(QEI_CONFIG_CAPTURE_A|QEI_CONFIG_NO_RESET|QEI_CONFIG_CLOCK_DIR|QEI_CONFIG_NO_SWAP),0);
//* 设置速度检测周期为 0.01秒
ROM_QEIVelocityConfigure(QEI1_BASE, QEI_VELDIV_1, 60000);
ROM_QEIEnable(QEI1_BASE);
ROM_QEIVelocityEnable(QEI1_BASE);
// Loop forever while the timers run.
while(1)
{
//* 读出上一个周期的速度计数值 */
i = ROM_QEIVelocityGet(QEI1_BASE);
/* 转化为 转/分钟*/
i = (i*100*60)/(4*512);
//读取当前方向
j1 = ROM_QEIDirectionGet(QEI1_BASE);
j1=j1;
ROM_SysCtlDelay(150*(ROM_SysCtlClockGet()/3000)); //DELAY 150MS
}
以上仿真时候i ,j1 没反映 ;为什么?请FAE指点