LM3S9B96上用GIMP做图形后,如果转换为M3的源码



哪里有GIMP转换到LM3S9B96上的教程

  • 1. Find a picture, for example, you can fine one in the C:\StellarisWare\boards\dk-lm3s9b96\qs-checkout\ram_html\thumbnail  7-capitol.jpg

    2. 7-capitol.jpg is 75*75 in size and is a RGB image.

    3. Convert the RGB color image to Index color image(256 color)

    4. Convert the Index color image to a PNM image

    5. Generate a “c” array with the PNM tool, you can find it in C:\StellarisWare\tools\bin\pnmtoc.exe

    6. Run pnmtoc in a DOS command window, something like" pnmtoc -c yourinput.pnm > output.h"

    7. Add the generated C array into project and run