LM3S9B96 -IQC80B1 can not Download program

Other Parts Discussed in Thread: SEGGER

MY second procurement is B1 Version.When welding on my board,it can not been download. In order to eliminate the said online that download cause lock , I use SEGGER's J_Link  to test a new and  without download operation over IC. The report shows: unvilid JTAG ID, can not find core.

But I use the last purchase version of C5, everything is normal.This ruled out my circuit board design problems. I think  different version lead to download failed, for the LM3S9B96-B1 version , how to correctly operate I need  help, thank you!

 

  • Have you checked the if the IC is damaged?

    As I know, B1 version has some issues on reset/power on (as shown in attached file, chapter 17). You can try to do some modification to your reset circuit and power supply and see if it helps.

    errata-LM3S9B96.pdf
  • 首先B1 的五片都是同样的问题,找不到内核(core),这个应该不会全坏。

    我根据勘误文件调整了复位阻、容值,(由于我直接用了片上LDO 供核心电压VDDC,上电时序就是默认的先VDD 在VDDC) 外接1.2V VDDC先供电,再上VDD(人为控制的差几秒) ....很遗憾,还是一样的问题。不知我这样上电Sequence是否可以。

    很感谢

  • 不知楼主的B1芯片多吗,是不是一定要用上?C5芯片会新一些能解决很多现有问题,如果可能尽量用C5版本吧

    楼主说的上电时序问题,可以用示波器看看,是否能够达到errata中要求那样?